The included IMAGE file can be used to construct Initio INI-9XXXU Driver 
Disk 2, SCO Unix/Unixware Manager Set v.2.31.  The included FCOPY.EXE 
can expand the IMAGE file to create a UNIX format disk.

How to Use It: 

1.  Unzip the downloaded 9XU230_2.ZIP file which produces three files:
    FCOPY.EXE
    9XU230_2.IMG
    README.TXT ( this file )
    
2.  Insert a DOS preformatted 3.5" 1.44MB floppy diskette into the drive a:

3.  Execute the following:  fcopy /f9XU231_2.IMG a:

4.  The Initio INI-9XXXU/9XXXUW Driver Disk 2 for SCO UNIX, UnixWare Rel. 
    2.31 is now created and ready to use.  This floppy is not readable on 
    DOS machines and only usable on UNIX OS.