|
 |
1.To
remove the cover of HUR1 unscrew and remove the screws on the
bottom of unit. Only one side (top) of screws needs to remove.
Top side is the side where power switch is. Insert the screw-driver
into the bolt and push upward to release the top cover.
|
 |
2.
Unfasten the screws on HDD holder case and pull backward to release
the HDD holder case.
|
 |
|
Since
using RAID1 (Mirror Mode) if install improperly, the HDD which already
contain DATA will be formatted. To prevent Data lost please follow
step 3-1 for installing under RAID 1 (Mirror Mode) |
|
| Installing
Single or RAID0 Mode |
 |
| |
3.Insert
both HDD1 and HDD2 into both bays of HDD holder and secure them with
screws. |
 |
| |
4.Insert
back the HDD holder back to HUR1 with both HDDs attached. |
 |
| |
5.Push
forward the HDD holder to secure the connection and fasten the screws
on the holder. |
 |
| |
6.Recover
the top plate of HUR1 and fasten the screws prior remove.
Now
installation is complete, please attach power core and connect HUR1
with USB cable to computers. HUR1 is ready to use. |
 |
|
|
| Installing
RAID1 Mode |
 |
 |
Installing
this method, if first HDD already contain data. Note: Two
HDDs must be identical in brand, size and model number. |
| |
3-1.
Insert first HDD which contain data. And fasten with screws. |
 |
| |
3-2.
Insert back the HDD holder back to HUR1 with first
HDDs attached. Make sure the connection of HDD holder
and HUR1 is intact. |
 |
| |
At
this point, please connect HUR1 to power source and turn on the unit.
(no need to connect to computer.) HUR1 will automatically build a
RIB table to First HDD. This way is for HUR1 to recognize the source
HDD. After the RIB table is written on to HDD, the error light indicator
of second HDD will light. Power off and remove the HDD holder to install
the second HDD. |
|
| |
3-3.
Please insert second HDD and secure it with screws. |
 |
| |
3-4.
Push forward the HDD holder to secure the connection and fasten the
screws on the holder. |
 |
| |
3-5.
Recover the top plate of HUR1 and fasten the screws prior remove.
Now
installation is complete, please attach power core. After turn on
the unit, HUR1 will perform “REBUILT” function. This copies an identical
data from HDD1 to HDD2. Rebuilt can be done off-line. After Rebuilt
indicator LED goes off and HUR1 is ready to use. Rebuilding data
might take several hours depend on the capacities of HDDs. |
 |
|
| System
Setup Connection
to your computer |
 |
| |
Few
cautions before using RAID enclosure
1.
Do not cover or block the ventilation holes on the enclosure.
2.
Check for visible damage on unit, accessories and cables before
tuning on the power.
3.
Do not expose the enclosure to water and humid conditions. |
| |
|