| Macintosh
Before connecting to the Macintosh please refer to our Hard Drive
Assembly procedures for RAID set-up.
If HDD is pre-installed by our vendor, user can plug directly to
Macintosh and start using the unit. If wish
to change the setting please refer to Hard Drive Assembly for correctly
way of setting.
Turn on Macintosh and start Mac OS.
Connect (USB or FIREWIRE-1394) HUR1 and turn on the power.
Mac OS will search and install drive automatically.
External drive will appear on Desk top.
Remove
the “external hard drive” from Macintosh..
Drag the external hard drive to trash bin.
Turn off the power.
Note:If
user wishes to use HUR1 on both Windows and Mac OS system, we recommend
that HDD to be formatted at FAT32. Also, please do the formatting
under Windows OS. If formatting is done by Mac OS, Windows might not
recognize the drive.
Our recommendation of file systems to be formatted on HDD:
Before
connecting to the Macintosh please refer to our Hard Drive Assembly
procedures for RAID set-up.
If HDD is pre-installed by our vendor, user can plug directly to
Macintosh and start using the unit. If wish to change the setting
please refer into Hard Drive Assembly for correctly way of setting.
Turn on Macintosh and start Mac OS.
Connect (USB or FIREWIRE-1394) HUR1 and turn on the power.
Mac OS will search and install drive automatically.
External drive will appear on Desk top.
Remove
the “external hard drive” from Macintosh..
Drag the external hard drive to trash bin.
Turn off the power.
‧Note: If user wishes to use HUR1 on both Windows and Mac
OS system, we recommend that HDD to be formatted at FAT32. Also,
please do the formatting under Windows OS. If formatting is done
by Mac OS, Windows might not recognize the drive.
Our recommendation of file systems to be formatted on HDD:
Win2000, Win XP, Vista
NTFS
Mac OS X HFS+ (Mac
OS Extended)
Both Windows and Mac OS
FAT32 |