SUNIX Inc. Multi-I/O Controller Windows(R) Driver.

******************************************************************************
This driver is built for the Microsoft(R) Windows Operating Systems.

Copyright 2010 SUNIX, Inc. All names mentioned herein are a registered trademark 
 or a trademark of SUNIX or its respective owners. All rights reserved.
******************************************************************************

Driver Version : 7.2.0.0

Release Data : 2010/12/07

******************************************************************************
SUPPORT PLATFORM:

Windows 7 32bit/64bit
Windows Vista 32bit/64bit
Windows XP 32bit/64bit
Windows Server 2008 R2 64bit
Windows Server 2008 32bit/64bit
Windows Server 2003 32bit/64bit
Windows 2000 SP4
Windows Embedded POSReady 2009


******************************************************************************
SUPPORT PRODUCT LIST:

SER4027A, SER4027P, SER4027D,
SER4037A, SER4037D, SERMSL2010HP, SER4437A, SER4456AM/LM/PM/LL, SER4466RM, SER4337AM,
SER4056A, SER4056P, SER4056AM/LM/PM/LL, SER4056HP, SER4056VL/LV, SER4056DW, SER4056JM,
SER4000A/AL/P/PL, SER4356AM,
SER4066A, SER4066EM, SER4066LL/LV, SER4066WN, SER4066RM, SER8000A, SER8000AL, SER4366AM,
SER1600A, SER1640A,

PAR4008A, PAR4018A, PAR4418A, PAR4008AT, PAR4018AT, PAR4008LV/LL,

MIO4469FX, MIO4079A, MIO4079AT, MIO4479FX, MIO4089A, MIO4089AM, MIO4097A, MIO4096AM,

SER4400A/AL/P/PL, SER8400A, SER8400AL,

SER5027A, SER5027AL, SER5027H, SER5027HL, SER5027P, SER5027PL, SER5027PH, SER5027PHL,
SER5027U, SER5027UL, SER5027UH, SER5027UHL,
SER5037A, SER5037AL, SER5037H, SER5037HL, SER5037P, SER5037PH, SER5037PL, SER5037PHL, 
SER5037U, SER5037UL, SER5037UH, SER5037UHL, SER5037B,
SER5056A, SER5056AL, SER5056H, SER5056HL, SER5056P, SER5056PL, SER5056PH, SER5056PHL,
SER5056U, SER5056UL, SER5056UH, SER5056UHL, SER5056J, SER5056PZ, SER5056WN, SER5056HP,
SER5066A, SER5066AL, SER5066H, SER5066HL, SER5066U, SER5066UL, SER5066UH, SER5066UHL,
SER5066LL, SER5066RK, SER5066WN, SER5066J, SER5066JH,

SER5337A, SER5356A, SER5366A,

SER5427A, SER5427AL,
SER5437A, SER5437AL, SER5437H, SER5437HL, SER5437P, SER5437PL, SER5437PH, SER5437PHL,
SER5456A, SER5456AL, SER5456H, SER5456HL, SER5456P, SER5456PL, SER5456PH, SER5456PHL,
SER5466A, SER5466AL, SER5466H, SER5466HL,

PAR5008A, PAR5008AL, PAR5008T, PAR5408A, PAR5408AL,

MIO5069A, MIO5069H, MIO5069P, MIO5069HP, MIO5069U, MIO5069UL, MIO5069UH, MIO5069UHL,
MIO5069T, MIO5469A, MIO5469H,
MIO5079A, MIO5079B, MIO5079H, MIO5079AL, MIO5079HL, MIO5079U, MIO5079UL, MIO5079UH,
MIO5079UHL, MIO5079T, MIO5479A, MIO5479H, MIO5479AL, MIO5479HL,
MIO5099A, MIO5099H, MIO5499A, MIO5499AL, MIO5499H, MIO5499HL,

IPC8139SI, IPC8159SI, IPC8169SI,
IPC-P1002, IPC-E1002, IPC-B1002, IPC-P1004, IPC-E1004, IPC-B1004,
IPC-P1008, IPC-E1008, IPC-B1008, IPC-P1016,
IPC-P2002, IPC-P2002SI, IPC-E2002, IPC-E2002SI, IPC-B2002, IPC-B2002SI,
IPC-P2004, IPC-P2004SI, IPC-E2004, IPC-E2004SI, IPC-B2004, IPC-B2004SI,
IPC-P2008, IPC-P2008SI, IPC-E2008SI,
IPC-P3004, IPC-E3004, IPC-P3008,
IPC-E1102, IPC-E2102SI, IPC-E1104, IPC-E2104SI, IPC-P2102, IPC-P2102SI,
IPC-P2104, IPC-P2104SI, IPC-P2108, IPC-P2108SI, IPC-E2108, IPC-E2108SI, IPC-P2116,
IPC-P3104, IPC-P3104I, IPC-E3104, IPC-E3104I, IPC-P3108, IPC-P3108I, IPC-E3108, IPC-E3108I,

CBS1009, CBS2009, CBS4009, CBS1000, CBS2000, CBS4000, CBP1000, CBP0010M, CBP0020M,
CBM1925, CBM2925, CBM1010, CBM2010,

ECS1400, ECS2400, ECS4400, ECS1000, ECS2000, ECS4000, ECP1000, ECM1010, ECM1020,

CDK1037A, CDK1037N, CDK1056A, CDK1056N, CDK1066A, CDK1066N,

DIO0601A, DIO0801A, DIO1601A, DIO3201A, DIO0601H, DIO0801H, DIO1601H, DIO3201H,
DIO0601P, DIO0801P, DIO1601P, DIO3201P, DIO0601PH, DIO0801PH, DIO1601PH, DIO3201PH,
DIO0601AL, DIO0801AL, DIO1601AL, DIO3201AL, DIO0601HL, DIO0801HL, DIO1601HL, DIO3201HL,
DIO0601PL, DIO0801PL, DIO1601PL, DIO3201PL, DIO0601PHL, DIO0801PHL, DIO1601PHL, DIO3201PHL,
DIO0602A, DIO0802A, DIO1602A, DIO3202A, DIO0602H, DIO0802H, DIO1602H, DIO3202H,
DIO0602P, DIO0802P, DIO1602P, DIO3202P, DIO0602PH, DIO0802PH, DIO1602PH, DIO3202PH,
DIO0602AL, DIO0802AL, DIO1602AL, DIO3202AL, DIO0602HL, DIO0802HL, DIO1602HL, DIO3202HL,
DIO0602PL, DIO0802PL, DIO1602PL, DIO3202PL, DIO0602PHL, DIO0802PHL, DIO1602PHL, DIO3202PHL,
DIO0604A, DIO0804A, DIO1604A, DIO3204A, DIO0604H, DIO0804H, DIO1604H, DIO3204H,
DIO0604P, DIO0804P, DIO1604P, DIO3204P, DIO0604PH, DIO0804PH, DIO1604PH, DIO3204PH,
DIO0604AL, DIO0804AL, DIO1604AL, DIO3204AL, DIO0604HL, DIO0804HL, DIO1604HL, DIO3204HL,
DIO0604PL, DIO0804PL, DIO1604PL, DIO3204PL, DIO0604PHL, DIO0804PHL, DIO1604PHL, DIO3204PHL,
DIO0608A, DIO0808A, DIO1608A, DIO3208A, DIO0608H, DIO0808H, DIO1608H, DIO3208H,
DIO0608P, DIO0808P, DIO1608P, DIO3208P, DIO0608PH, DIO0808PH, DIO1608PH, DIO3208PH,
DIO0608AL, DIO0808AL, DIO1608AL, DIO3208AL, DIO0608HL, DIO0808HL, DIO1608HL, DIO3208HL,
DIO0608PL, DIO0808PL, DIO1608PL, DIO3208PL, DIO0608PHL, DIO0808PHL, DIO1608PHL, DIO3208PHL,


******************************************************************************
RELEASE NOTE:

Ver 7.2.0.0 - 2010/12/07
    0)  release version
    1)  support internal/external GPIO
    2)  support 3-in-1 (RS-232/422/485) series
    3)  support more than three parallel ports
    4)  support SUNIX cash drawer kicker interface card
    5)  support SUNIX serial library
    6)  support multi-language UI
    7)  support silent installation
    8)  modify layout of control page
    9)  use driver dll to replace system default dll
   10)  fix an issue about H/W flow control setting in RS-422/485
   11)  fix an issue about the delay time of closing port
   12)  fix an issue about driver crash during change power state
   13)  fix an issue about buffer overflow

Ver 7.1.0.0 - 2010/01/13
    0)  release version
    1)  solve an issue about re-map series
    2)  support SUN1999 cardbus series
    3)  modify layout of control page
    4)  add reference clock setting in control page
    5)  add specific IoControl command to return part number

Ver 7.0.0.0 - 2009/07/14
    0)  release version
    1)  support Golden series, Matrix series, and SUN1999 series


******************************************************************************
INF FILES:

	snxpci.inf:	SUNIX multi-function card driver INF file
	snxpcip.inf:	SUNIX serial/parallel port driver INF file


******************************************************************************
INSTALLATION AND REMOVAL INSTRUCTIONS:

------------------------------------------------------------------------------
Using Driver Installation Package to install SUNIX Multi-I/O Controller Driver

Note: It is always best to remove any previously installed Multi-I/O Card 
       Driver from the system before installing a new driver.

1. Browse to the driver files location and double click Setup.exe.

2. When installing, the driver install dialog box appears. Click on the Next, 
    Continue, or OK prompts to complete the installation when they appear.


------------------------------------------------------------------------------
Remove SUNIX Multi-I/O Controller Driver from Add/Remove Programs (Windows XP)
 or Programs and Features (Windows Vista later)

1. Open Control Panel, double-click on the Add/Remove Programs
   (or Programs and Features) icon in it.

2. Click on SUNIX Multi-IO Controller, select Remove, and then press Next
   to uninstall it.

3. Reboot the system to uninstall the driver fully.


------------------------------------------------------------------------------
Using silent installation command to install SUNIX Multi-I/O Controller Driver

1. Open Command Processor, find the driver path.

2. Run "Setup.exe /s /f1<path\setup.iss> /f2<path\LogFile>"
   i.e. Setup.exe /s /f1C:\SUNIX_driver\setup.iss /f2C:\LogDir\LogFile.log


------------------------------------------------------------------------------
Remove SUNIX Multi-I/O Controller Driver using silent installation command

1. Open Command Processor, find the driver path.

2. Run "Setup.exe /uninst /f1<path\uninst.iss> /f2<path\LogFile>"
   i.e. Setup.exe /uninst /f1C:\SUNIX_driver\uninst.iss /f2C:\LogDir\LogFile.log

3. Reboot the system to uninstall the driver fully.