RAYON  MultiPort P984 Adapter  DOCUMENTATION FOR NT
               ---------------------------------------------------

   DRIVER INSTALLATION

      If you currently have a P984 driver installed, please remove it .After
      removing the driver, reboot your system.  This is necessary because
      NT will not allow a new driver to be installed until the driver
      is unloaded from memory.

        Once Windows NT has started, login using an account which has
        administrative rights.  Start the Control Panel applet by double-
        clicking it icon in the Program Managers main group.  In the
        Control Panel applet, double-click the network icon to bring up
        the Network Control Panel Applet (NCPA).  Within the NCPA, select
        the Add Adapter button.  A list of possible adapters should be
        displayed.

                Go to the end of the list and select:
                        '<Other> Requires disk from manufacturer'

        When prompted for the path, specify the drive and directory where
        the NCPA can find the new driver for the platform you are installing.

                For example, if you were installing from your drive A: floppy
                diskette:
                                a:\p984\nt4

        The important thing to remember is to supply the correct directory.

      You can now follow the configuration dialog boxes to finish installing
        the P984 Driver.
