[Driver Version: 1.16.47.2 to 1.16.60.1] 1. Added ASM3142 Support [Driver Version: 1.16.47.1 to 1.16.47.2] 1. Version 1.16.47.2 : INF file with Co-Installer 2. Add customized 4 parts ID for Windows Update. [Driver Version: 1.16.46.1 to 1.16.47.1] 1. Support Windows 10 RS2 2. Fix Touch monitor E230T detection failure 3. Fix Thunderbolt System BSOD when S3/S4 resume or Thunderbolt PnP 4. Version 1.16.47.1 : INF file with Copy INF 5. Add customized 4 parts ID for Windows Update. [Driver Version: 1.16.45.1 to 1.16.46.1] 1. Modify Inf to install driver on windows update 2. Add USB device recovery resuming from S3 for thunderbolt 3. Modify wait-wake mechanism for USB Ethernet device 4. Add customized 4 parts ID for Windows Update. [Driver Version: 1.16.44.1 to 1.16.45.1] 1. Thunderbolt System occurs Black Screen after the system resumes from S3 2. ASM1142 displays external hub in device manager after installing 1.16.41.3 driver version 3. Add customized 4 parts ID for Windows Update. 4. Improved ADATA UC350 USB pen drive S3 resume detection rate on charger port. [Driver Version: 1.16.43.1 to 1.16.44.1] 1. Sandisk Cruzer Glide 3.0 pen drive is lost while Thunderbolt System resuming from S3 2. Thunderbolt System occurs Black Screen after the system resumes from S3 [Driver Version: 1.16.42.1 to 1.16.43.1] 1. Thunderbolt System occurs function abnormality in device manager with quickly hot plug [Driver Version: 1.16.41.3 to 1.16.42.1] 1. S4 will BSOD 0x7E with Thunderbolt Docking. 2. Cannot found host in USB root hub by USB View while connecting up to two hosts. 3. Add customized 4 parts ID for Windows Update. 4. Only support ASM2142 under Win7. 5. Improve performance by changing memory map DMA setting [Driver Version: 1.16.40.1 to 1.16.41.3] 1. Add customized 4 parts ID for Windows Update. 2. Remove patch: Intel Alpine Ridge Thunderbolt +on board ASM1042A system with USB3.0 Realtek RTL8153 LAN running cold boot and warm boot shows BSOD. 3. There is reinstall failure rate of the class driver after hot plug Thunderbolt. 4. The System with USB LAN Dongle fails to wake on LAN from S3. [Driver Version: 1.16.39.1 to 1.16.40.1] 1. Intel Alpine Ridge Thunderbolt + on board ASM1042A system with Realtek USB3.0 RTL8153 LAN running cold boot and warm boot shows BSOD. [Driver Version: 1.16.38.1 to 1.16.39.1] 1. Intel Alpine Ridge Thunderbolt + on board ASM1042A system with Realtek USB3.0 RTL8153 LAN idling 2~3hrs shows BSOD. [Driver Version: 1.16.37.1 to 1.16.38.1] 1. Onboard Intel USB host doesn’t work and shows a yellow exclamation mark in device manager after install 1.16.37.1 [Driver Version: 1.16.36.1 to 1.16.37.1] 1. Intel Alpine Ridge Thunderbolt + on board ASM1042A system idling from S3 resume shows BSOD. 2. The LED flickers after USB pen drive is ejected. 3. 1.16.36.1 install shield fails to install in Vista. [Driver Version: 1.16.35.1 to 1.16.36.1] 1. Support ASM2142 2. System occurs BSOD while PnP Asix MCS7715 (USB1.1 to Single Serial and Single Parallel controller device) 3. Add customized 4 parts ID for Windows Update. [Driver Version: 1.16.34.2 to 1.16.35.1] 1. Add customized 4 parts ID for Windows Update. 2. Enhance performance 3. Fail to update Root Hub Controller driver by Windows Update. 4. Win7 device manager cannot find USB1.1 keyboard/mouse and system cannot shut down after install “Citrix Receiver”. [Driver Version: 1.16.34.1 to 1.16.34.2] 1. Fix 1.16.34.1 bug: Connect a hub under Windows 10 shows yellow mark. [Driver Version: 1.16.33.1 to 1.16.34.1] 1. Add customized 4 parts ID for Windows Update. 2. Synchronize the string as inbox driver in system manager. [Driver Version: 1.16.32.1 to 1.16.33.1] 1. System always rescans with GL3520 USB3.0 Hub behind Dell Trinity Docking (ASM1042A + SMSC Hub). 2. An Oculus Rift Camera hangs when running multiple Oculus Rift Cameras (Etron Solution) with Oculus Rift Camera tool. [Driver Version: 1.16.31.1 to 1.16.32.1] 1. Support Device Guard. [Driver Version: 1.16.30.1 to 1.16.31.1] 3. USB device cannot be detected with Non-HDD System via Ethernet. 4. RJ45 port is disconnected after PnP Realtek USB LAN (RTL8153AD) cable from Dell Trinity Docking (ASM1042A + SMSC Hub). 5. System occurred BSOD while running S3 Stress test with Dell Trinity Docking (ASM1042A + SMSC Hub). 6. HornetTek USB3.0 Super Slim Portable Blu-Ray Burner (HT-OBW01B-U3) behind Dell Trinity Docking (ASM1042A + SMSC Hub) cannot be detected on USB2.0 port. 7. Dell Trinity Docking (ASM1042A + SMSC Hub) re-enumerated from S4 resume. 8. Add customized 4 parts ID for Windows Update [Driver Version: 1.16.29.1 to 1.16.30.1] 1. The Power DVD could not play after plug ASUS BW-12D1S-U ODD on ASM1142. 2. Add customized 4 parts ID for Windows Update [Driver Version: 1.16.28.1 to 1.16.29.1] 1. Support multiple languages installation: Korean/Dutch/ German/ Italian/ Swedish 2. PnP HP Trump Docking (ASM1042A + ASM1074) caused System random BSOD 3. Add customized 4 parts ID for Windows Update [Driver Version: 1.16.27.1 to 1.16.28.1] 1. ASM1142 couldn't be recognized USB device when S4 resume 2. Add customized 4 parts ID for Windows Update [Driver Version: 1.16.26.1 to 1.16.27.1] 1. Fix WHLK test items Mutt TCD1~TCD9 random fail [Driver Version: 1.16.25.1 to 1.16.26.1] 1. Support Windows 10 [Driver Version: 1.16.24.0 to 1.16.25.1] 1. Disconnected Intel 3D camera is still visible in device manager 2. USB keyboard irock KR-6260-WE and FOXXRAY Fury Howling (FXR-BK-03) gaming keyboard cannot be detected on Windows 7 3. Creative Sound Blaster E1 sound card became louder from S4 resume 4. USB3.0 device on ASM1142 shows "This device can perform faster" after power surge 5. Rename driver naming string: ASM1142 as “ASMedia USB3.1 eXtensible Host Controller” ASM1042 / ASM1042A series as “ASMedia USB3.0 eXtensible Host Controller” 6. ASUS pad TF701T detection fail from S4 resume on Z97-E/USB3.1 platform 7. Set ASMedia driver as higher priority of installation than Microsoft inbox driver 8. Support multiple languages installation: English/Chinese (Traditional)/Chinese (Simplified) French/Portuguese/Brazilian/Spanish/Japanese [Driver Version: 1.16.23.0 to 1.16.24.0] 1. System fail to enter S3 when connect the pen drive under ASM1142 downstream port in ASUS X99 Pro [Driver Version: 1.16.22.0 to 1.16.23.0] 1. Fix ASM1142 Over current event could not pop up. 2. When ASM1142 with device link at USB3.1 10G speed, OS will show down mode message if Intel USB driver installed. 3. Enhance ASM1142 performance. 4. There is noise when playing music with ASUS STRIX headset (CMedia USB audio chip) in ASM1042A USB3.0 port (Note: add new VID/DID) 5. Fix ASUS NB G771JMC (ASM1042A) + Intel 3D camera occurred BSOD with driver version 1.16.22.0. 6. Fix ASUS NB G771JMC (ASM1042A) + Intel 3D camera factory function test – HDD swap fail 7. Fix ASM1042A cannot play audio normally with ASUS APPAndroid Open Accessory 1.00.04 8. Fix ASM1042AE cannot recognize MI tablet and ASUS TF701 tablet [Driver Version: 1.16.19.0 to 1.16.22.0] 1. ASUS Data and KVM sharing cable cannot be used with ASM1042AE. 2. Performance drop when copying a file to two WD MyPassport USB3.0 HDD (bridge: JM) and (bridge: Initial) at the same time on X99 platform with USB3.0 Boost enabled. 3. Enable xHCI 1.1 function. 4. Fix Intel 3D camera hang when record video with Win8.1 Metro Camera. [Driver Version: 1.16.18.0 to 1.16.19.0] 1. System occurred BSOD by reading or writing files to LiteOn DVD Player in Windows 7 embedded OS. [Driver Version: 1.16.16.0 to 1.16.18.0] 1. Copy 1GB file lag with Apacer pen drive [Driver Version: 1.16.15.0 to 1.16.16.0] 1. Multiple Thunderbolts connection – mouse could not be recognized: Keyboard / mouse cannot be detected when link to PC USB2.0 Host or Mac USB3.0 Host) [Driver Version: 1.16.12.0 to 1.16.15.0] 1. Plug TRIPP-LITE-U336 USB3.0 TO ETHERNET-0214 into ASM1042A and install device driver at Win8, Windows icon would show disconnection but it can be recognized by Windows Device Management. [Driver Version: 1.16.9.0 to 1.16.12.0] 1. ASM1042/1042A with ASM1074 hub on ASUS X79-Deluxe cannot get WHQL with Win7 64bit . [Driver Version: 1.16.4.0 to 1.16.9.0] 1. Cannot capture frame when ASM1042 was with SkyDigital SKYTV USB 3.0 HDMI capture device. 2. S3 resume needs to wait 30sec when Brother MFC-J625DW printer plugged in ASM1042 with VL810 Hub. 3. Fix driver would occur system crash issue (0x9F). 4. Plug in AZIO USB2.0 Bluetooth BTD-V201 to ASM1042 with VL810 hub then the device cannot be recognized. 5. Plug in Billiontion GUBTCR41J-BI-GL Bluetooth adapter to ASM1042 with VL810 hub cannot be recognized. 6. Plug 10MOONS-T24-0036 Web CAM to ASM1042 and run AMCap.exe_V9.00, after plug-out then plug-in the device would flicker. [Driver Version: 1.16.3.0 to 1.16.4.0] 1. PQI H567V pen drive lost after OS restart. 2. Install USB 3.0 ODD Samsung SE-S084D after Win 8 OS installation caused BSoD with inserting DVD disk. 3. HITACHI TURBO MOBILE PRO 500G showed "Hardware ID Missing" when user changed U3 boost setting. 4. AgStar 3UB3A8 plug in ASM1074 Hub was lost after S3 resume. 5. Asus Xonar Essence One Audio device: speed mode down from HS to FS when it plugged in ASM1074 Hub. 6. Asus Xonar Essence One Audio device: FW Update Tool cannot be recognized. [Driver Version: 1.16.2.0 to 1.16.3.0] 1. Cannot ping with AXIS AX88179 USB 3.0 to Gigabit Ethernet card successfully with ASM1042. 2. UASP write performance of CyberSlim S2-U3 Turbo was abnormal with U3 Boost 1.03.02. (Note: Need to match with ASM1042 firmware version 120927_01_02_00) [Driver Version: 1.16.1.0 to 1.16.2.0] 1. System cannot enter S3/S4 under Windows 8 RTM. 2. USB3.0 device got lost or rescan after S3 resume under Windows 8 RTM. [Driver Version: 1.14.10.0 to 1.16.1.0] 1. ASUS AK1D keyboard / AM1D mouse was lost after resuming from S3/ S4. 2. xHCI 1.0 support. 3. TP Link WN821N / WN722N shows yellow mark in device management. 4. MIS tool shows two device when connects IEI dongle SM325 behind USB3.0 hub which is under ASM1042 down port. 5. All-in-One A14HV occurs BSOD when shuts down with battery mode. 6. ASUS USB3.0 docking was lag with video burn-in test in ASUS K53S/U24E/U82U Notebook. 7. Fix WHCK 2.0 test - USB Exposed Port Controller Test fail 8. Fix WHCK 2.0 test - USB xHCI Runtime Power Management Test fail [Driver Version: 1.14.9.0 to 1.14.10.0] 1. Fix yellow exclamation mark of mass storage device on Win 8 64bit OS. [Driver Version: 1.14.8.0 to 1.14.9.0] 1. This driver version supports Displaylink USB3.0 to Video devices with Displaylink driver version 6.2.37116 2. UAS performance with Cyberslim S1-U3 turbo is lower than BOT mode in F1A75-V Pro platform with onboard ASM1042 (PCIe slot from SB) [Note] This issue is solved to match with host firmware version 120406_00_02_63 3. Cannot install TELSTRA USB 4G dongle driver (Sierra Wireless AirCardR 320U) successfully in USB3.0 port and shows device unplugged message. [Driver Version: 1.14.4.0 to 1.14.8.0] 1. The USB3.0 performance with USB3.0 Flash Corsair Voyager GT USB3 in P9X89 Deluxe (ASM1042 host) is worse than in C4F (NEC host) 2. 3G dongle ZTE MF633 is no internet signal from S4 resume. 3. 3G dongle BandLuxe has no response from S4 resume. System cannot execute 3G AP when device fail. Re-plug device is ok. 4. 4G dongle TELSTRA USB (Sierra Wireless AirCardR 320U) occurs BSoD when install dongle driver in USB3.0 port. 5. Do nothing to DUT then suspend to enter S3/S4, USB3.0 device rescan in ASUS P8Z68 V/Gen3 USB3.0 Device List: CyberSlim S1-U3S Seagate FreeAgent GoFlex 500GB STAA500305 6. System cannot wake up from S3 and S4 with SILVERSTONE SST RVM01B USB gaming mouse behind VLI hub [Driver Version: 1.14.3.0 to 1.14.4.0] 1. There is pop-noise with ASUS Xonar Essence One USB audio amp during playing audio. 2. Playing audio caused AP hang with ASUS Xonar U1 USB station. [Driver Version: 1.14.2.0 to 1.14.3.0] 1. Pull-out Alcor AU-9540 smart card reader after entering suspend-mode, the device still existed in device manager and caused ASM1042 not functioning. 2. SilverStone SST RVM01B mouse remote wake-up failed via ASM1042. 3. USB devices needed 30 seconds to function after entering Win PE. 4. Improve resuming time via hub to fix WHQL test failure. [Driver Version: 1.14.1.0 to 1.14.2.0] 1. Upgrade driver version code: To synchronize the version codes on different release branches, version code from this release is updated to v1.14.x.x 2. The "power management tab" always appears whatever the option "S3 wake up-BIOS" is enabled or disabled 3. Connect VLI hub to USB3.0 root port, disable then enable the VLI Hub stack. System fails to enable. [Driver Version: 1.12.9.0 to 1.14.1.0] 1. System occurs BSOD when re-plug Dell USB Keyboard SK-8135 in USB3.0 port. 2. System occurs BSOD when execute Win PE to recovery system in ASUS AIO (G440 CPU) Platform. 3. Plug-in TP-Link wireless LAN card TL-WN722N in USB3.0 port shows yellow mark in device manager after installing device driver. 4. Device missing in aging reboot test (Resuming from suspend) in ASUS X79 Platform. 5. There will be fail rate to detect USB2 device via USB3 VLI Hub VLI810 in aging reboot test. [Driver Version: 1.12.5.0 to 1.12.9.0] 1. Support spin down function 2. Plug-in Getac PDA PS236 shows yellow mark in device manager after mobile center 6.1 driver installation. 3. Support save-restore function 4. Keyboard and mouse S3 wake up fail in MS-AC75 after resuming S4 done 5. Cannot recognize WiBro Modem (SWD-H300K) and shows yellow mark in device management 6. System resuming from S3/S4 occurs BSoD with USB to Serial converter cable plug-in USB 3.0 port 7. System can not recognize USB2.0 device with ASUS AiCharger [Driver Version: 1.12.5.0] 1. Plug in AD370 TV turner in USB3.0 port will cause system crash after install AD370 driver and application software. 2. Cancel the power management option of XHCI driver “allow this device to wake the computer”, system still can be woke up by S3/S4. 3. The OS XP will show yellow mark after install USB to COM port device driver (Prolific PL-2303HXD). 4. The system first time S3 wake-up fail with MSI StarType ES500 keyboard. 5. Improve system stability