##########Realtek WLAN Driver Install Package################## Language Support ¡G 1->English 2->Basque 3->Bulgarian 4->Catalan 5->Simple Chinese 6->Traditional Chinese 7->Croatian 8->Czech 9->Danish 10->Dutch 11->Finish 12->French(Canada) 13->French(France) 14->German 15->Greek 16->Hungarian 17->Indonesian 18->Italian 19->Japanese 20->Korean 21->Norwegian 22->Polish 23->Portuguese(Brazil) 24->Portuguese(Portugal) 25->Romanian 26->Russian 27->Serbian(Cyrillic) 28->Slovak 29->Slovenian 30->Spanish 31->Swedish 32->Thai 33->Turkish -- How to install: 1. Enter the directory and run setup.exe. 2. Follow the prompt and restart the system. --How to Silent Install: 1. Enter the directory and run setup.exe /s -f2"c:\setup.log" under command line. 2. Or execute silent install Batch file. -- How to Silent un-install: 1. Enter the directory and run Setup.exe -uninst -s -f1"(Uninstall.iss Path)" -f2"c:\setup.log" under command line. p.s. The (Uninstall.iss Path) is the full path of the file ¡§Uninstall.iss¡¨. For example , the full path of Uninstall.iss is ¡§c:\Realtek\11n USB WLAN Card¡¨ .The command will become Setup.exe -uninst -s -f1"(Uninstall.iss Path)" -f2"c:\setup.log" 2. Or execute silent uninstall Batch file. -- How to confirm driver version: 1. Right click computer->Manage->Device Manager. 2. Right click the Device Properties->Driver ######################################################## Release Note: ######################################################## InstallShield Drv V3.00.0001 (2016/04/26) By Karl_Hsu New [APP] FindRtl: V1.00.412.2016 (By Karl_Hsu) Quick find support Realtek card to complete the Driver .inf input output FindRtl.ini. SetDrvAll: V1.00.422.2016 (By Karl_Hsu) Support check unplug or plug in card installation, support WinXP ~ Win10 OS Install [Protocol Driver] Eappkt: V500.1001.802.2007 for WinXP [Script_Functions] All New.(By Karl_Hsu) ######################################################### InstallShield Drv V3.00.0001 (2016/04/28) By Karl_Hsu UpDate [APP] SetDrvAll: V1.02.428.2016 (By Karl_Hsu) [Script_Functions] Add delete "Realtek" folder .(By Karl_Hsu) ######################################################### InstallShield Drv V3.00.0001 (2016/05/03) By Karl_Hsu [Script_Functions] UI with modifications "WlanUI".(By Karl_Hsu) ######################################################### InstallShield Drv V3.00.0002 (2016/06/01) By Karl_Hsu UpDate [APP] SwUSB (XP_Win8) : V500.1033.530.2016 (By Karl_Hsu) Fix USB mode switch service stop work issues. [Script_Functions] Support install/remove external power limit table files.(By Karl_Hsu) ######################################################### InstallShield Drv V3.00.0003 (2016/06/30) By Karl_Hsu UpDate [APP] SwUSB (XP_Win8) : V500.1034.630.2016 (By Karl_Hsu) Fix Sometimes did not do ReLinkProfile in Switch USB2.0/USB3.0 mode Process. ######################################################### InstallShield Drv V3.00.0004 (2016/07/04) By Karl_Hsu [Script_Functions] If InstallCiscoEAP or Install_IHV_Extensions is displayed Yes/No Reboot.(By Karl_Hsu) ######################################################### InstallShield Drv V3.00.0005 (2016/07/27) By Karl_Hsu UpDate [APP] FindRtl: V1.2.724.2016 (By Karl_Hsu) SetDrvAll: V1.3.724.2016 (By Karl_Hsu) Detect Devices do not need to find matching "&REV_". ######################################################### InstallShield Drv V3.00.0006 (2016/08/3) By Karl_Hsu [Script_Functions] Delete Old ISS InstallShield. ######################################################### InstallShield Drv V3.00.0007 (2016/08/29) By Karl_Hsu [Script_Functions] Package use customized setup.ico Bug Fixes. ######################################################### InstallShield Drv V3.00.0008 (2016/08/31) By Karl_Hsu [Script_Functions] Setup.icon did not put the time, the default icon is displayed. ######################################################### InstallShield Drv V3.00.0009 (2016/10/13) By Karl_Hsu add change the work path variable in batch file. ######################################################### InstallShield Drv V3.00.0010 (2016/10/31) By Karl_Hsu [Script_Functions] Fix Eappkt protocol does not start in WinXP OS. UpDate [APP] SwUSB (XP_Win8) : V500.1035.1031.2016 (By Karl_Hsu) Modify Query OID_802_3_CURRENT_ADDRES use too small Buffer Length in WinXP OS. ######################################################### InstallShield Drv V3.00.0011 (2016/11/08) By Karl_Hsu [Script_Functions] Fix can not update Wlan Driver issue because RtlWlanU inbox driver error automatically installed in the USB Composite Device in Win10 Rs1 system. UpDate [APP] FindRtl: V1.03.1108.2016 (By Karl_Hsu) SetDrvAll: V1.004.1107.2016 (By Karl_Hsu) ######################################################### InstallShield Drv V3.00.0012 (2016/11/18) By Karl_Hsu [Script_Functions] Uninstall:Modify the time to stop and start SwUSB. UpDate [APP] SwUSB (XP_Win8) : V500.1036.1111.2016 (By Karl_Hsu) Increase check card removal status at initialization Process. ######################################################### InstallShield Drv V3.00.0013 (2016/11/30) By Karl_Hsu UpDate [APP] SwUSB (XP_Win8) : V500.1037.1130.2016 (By Karl_Hsu) Fixes sometimes crash when exiting. ######################################################### InstallShield Drv V3.00.0014 (2016/12/09) By Karl_Hsu UpDate [APP] SwUSB (XP_Win8) : V500.1038.1209.2016 (By Karl_Hsu) Fixes a crash when a thread exits. ######################################################### InstallShield Drv V3.00.0015 (2017/05/24) By Karl_Hsu UpDate [APP] FindRtl: V1.04.502.2017 (By Karl_Hsu) SetDrvAll: V1.6.524.2017 (By Karl_Hsu) 1. Fixed when (EnumDeviceInfo size > 100) did not install the problem. 2. Fixed No card installed new driver problem when the Plug in the device card with the Inbox driver normal, And then remove the card. ######################################################### InstallShield Drv V3.00.0016 (2017/06/05) By Karl_Hsu UpDate [APP] SetDrvAll: V1.7.605.2017 (By Karl_Hsu) 1. Fixed Some platforms will crash when no card is installed. ######################################################### InstallShield Drv V3.00.0017 (2017/06/07) By Karl_Hsu UpDate [APP] SetDrvAll: V1.8.607.2017 (By Karl_Hsu) 1. The modification processing does not insert the card to update the Inbox driver. ######################################################### InstallShield Drv V3.00.0018 (2017/07/18) By Karl_Hsu UpDate [APP] SetDrvAll: V1.9.718.2017 (By Karl_Hsu) 1. Fixed Some platforms remove the Driver failed when Uninstall. ######################################################### InstallShield Drv V3.00.0019 (2017/10/17) By Karl_Hsu [Script_Functions] 1.Implement Extension INF install/remove. (By Karl_Hsu) #########################################################