v2.34.4 * First Release v2.34.6 * FIX: Hard drives interrupted during the erase process will cause machine malfunction. * NEW: After connected to PC if sanitizer is going to disconnect, then the screen will display message, ?Are you sure? ?. v2.35.7 * NEW: Improve HDD Compatibility. * FIX: Support for created a 3.5" Log Drive * FIX: Issue with updating/exporting a new log onto an existing log drive. * FIX: Formating issue with the LCD which prevented all text from being visible. v2.39.4 * CHANGED: Word choice modification. v2.42.8 * FIX: Perform “Enhanced Secure Erase” all will write 0. v2.43.0 * FIX: Secure erase unlock issue V2.43.1 * Fixed: Seagate Wolf 12TB hard drive cannot be recognize. (HDD from startup to ready require 20+ seconds) V2.43.4 * Fixed: After secure erase log report capacity will turn to 0MB. * Fixed: Perform Quick Erase then afterward perform Secure Erase, however it will only display Quick Erase's capacity. v2.43.6 * Fixed: If SSD got unplug during the erasing procedure, then it will result in FAIL immediately. * Fixed: After secure erase is interrupted. SSD will result in locked and restart secure erase process, the DCO will display correct size message.