--------------------------------------------------------------------- VIA USB 2.0 Host Controller Driver Package Release History --------------------------------------------------------------------- ============================== = Full Release Version 2.56 = ============================== * 2003/05/25 1. Fixed can't uninstall USB 2.0 hub from Device Manager under Windows XP SP1. 2. Fixed APLUX USB 2.0 WebCam can't work under Windows 2000. 3. Fixed compatiable issue with some PCMCIA CF card driver under WinME/98. 4. Added a new application to save remove VT6212 cardbus under WinME/98. ============================== = Full Release Version 2.55 = ============================== * 2003/05/14 (Ver 2.55) (No Released) 1. Driver v2.55 released. 2. Fixed the issue of APLUX USB 2.0 WebCam unable to work under Windows 2000. 3. Fixed the compatiable issue of some PCMCIA CF card drivers under WinME/98. 4. Added a new application to safely removed VT6212 cardbus under WinME/98. ============================== = Full Release Version 2.54 = ============================== * 2003/01/10 (Ver 2.54) 1. Driver v2.54 released. 2. Fixed the issue of APLUX USB 2.0 WebCam (Bulk) unable to work in WinMe/98. 3. Fixed some bulk devices with Cypress/In-System drivers unable to work in WinMe/98. 4. Fixed the problem of setup program not able to reboot in Windows XP SP1. ============================== = Full Release Version 2.53 = ============================== * 2002/12/06 (Ver 2.53) 1. Driver v2.53 released. 2. Fixed the problem of some USB CD-ROM can not be safely removed under Windows 98. ============================== = Full Release Version 2.52 = ============================== * 2002/11/14 (Ver 2.52) 1. Driver v2.52 released. 2. Fixed the problem of some USB CD-ROM can not be safely removed under Windows 2000. For Windows 2000, v2.51 will fail if the entire 1.1 USB host controllers are not enabled. This issue has been fixed in v2.52. ============================== = Full Release Version 2.51 = ============================== * 2002/10/31 (Ver 2.51) 1. Driver v2.51 released. 2. Fixed the problem of some USB CD-ROM can not be safely removed under Windows 2000. 3. Fixed the problem of some USB 1.1 low speed device can not be recognized under Windows 2000 and Windows XP. ============================== = Full Release Version 2.48 = ============================== * 2002/10/16 (Ver 2.48) 1. Driver v2.54 released. 2. Fixed the problem of some USB devices being reenumerated after resuming from S3 in Windwos 2000 and Windows XP. ============================== = Full Release Version 2.47 = ============================== * 2002/10/04 (Ver 2.47) 1. Driver v2.47 released. 2. Due to legal concerns, Microsoft EHCI driver stack for Windows XP from the package is remvoed. End users should go to Windows Update to download this driver or Service Pack 1. 3. Updated VIA USB 2.0 Host Controller Driver to fix the S3 suspend/resume issue in Windows 98. 4. Fixed Microsoft Internet Keyboard Pro with USB 2.0 Hub issue.(Version 4.90.3000.3) =============================== = Full Release Version 2.46A = =============================== * 2002/10/03 (Ver 2.46A) 1. Driver v2.46A released. 2. Modified SETUP.exe to support 2 EHCI controllers. 3. Modified SETUP.exe to support Silent Installation in Windows98 and Windows Me. ============================== = Full Release Version 2.46 = ============================== * 2002/08/30 (Ver 2.46) 1. Driver v2.46 released. 2. Modified SETUP.exe to fix WQHL issue in Windows XP Home Edition. ============================== = Full Release Version 2.45 = ============================== * 2002/08/29 (Ver 2.45) 1. Driver v2.45 released. 2. Modified SETUP.exe to Install driver in Windows 98 Gold. ============================== = Full Release Version 2.44 = ============================== * 2002/07/24 (Ver 2.44) 1. Driver v2.44 released. 2. Modified VIA USB driver INF file to pass signability test in Windows XP. 3. Modified SETUP.exe to fix some minor issues. ============================== = Full Release Version 2.42 = ============================== * 2002/07/04 (Ver 2.42) 1. Driver v2.42 released. 2. Modified VIA USB driver INF file to pass signability test in Windows 98 and Windows Me. ============================== = Full Release Version 2.41 = ============================== * 2002/06/25 (Ver 2.41) 1. Driver v2.41 released. 2. Updated Microsoft USB 2.0 Host Controller Driver for Windows 2000.(Version 5.0.2195.5652) ===================================== = Full Release Version 2.41 Beta 1 = ===================================== * 2002/06/20 (Ver 2.41 Beta 1) 1. Driver v2.42 released. 2. Updated VIA USB 2.0 Host Controller Driver to support both VT6202 and VT8235. (Version 4.90.3000.2) ============================== = Full Release Version 2.40 = ============================== * 2002/06/19 (Ver 2.40) 1. Driver v2.40 released. 2. Updated VIA USB 2.0 Host Controller Driver to support both VT6202 and VT8235.(Version 4.90.3000.1) ============================== = Full Release Version 2.24 = ============================== * 2002/04/19 (Ver 2.24) 1. Driver v2.24 released. 2. Updated Microsoft USB 2.0 Host Controller Driver for Windows XP. (Version 5.1.2600.41) ============================== = Full Release Version 2.23 = ============================== * 2002/04/18 (Ver 2.23) 1. Driver v2.23 initial public release.