//====================================================================== // ASIX MCS7832/MCS7830 Windows 8.x Drivers Setup Program // Revision History // // This document describes the major changes, additions and bug fixes made // to the program between released versions. //====================================================================== Note: ===== Before run the setup program to install newer driver, please uninstall the older driver that user installed before. User can check the list in "Control Panel" -> "Programs" -> "Programs and Features". If there is a MCS783x (MCS7832/MCS7830) driver in the list, uninstall it before run the setup program. Version 1.0.1.0 (2014-04-08) 1. This setup program includes the following MCS783x Windows 8.x 32-bit/64-bit drivers. MCS783x Windows 8.x 32-bit WHCK driver v1.16.1.0 MCS783x Windows 8.x 64-bit WHCK driver v1.16.1.0 2. Changed to shorter driver installed folder names and update a new product code. Version 1.0.0.0 (2013-01-21) 1. This setup program includes the following MCS783x Windows 8 32-bit/64-bit drivers. MCS783x Windows 8 32-bit WHCK driver v1.16.0.0 MCS783x Windows 8 64-bit WHCK driver v1.16.0.0 2. Built the setup program by using InstallShield2010 Premier from this verison.